AXIS#.SAFEPARAM.ACCCOMPUTATIONINTERVAL

Description

Indicates the time interval used to compute the acceleration in the SMM. This is only applicable when a safe encoder has been configured in the safety parameters.

Parameters Editor with the Acceleration Computation Time Interval circled

Context

For safe encoder details refer to Motor feedback requirements.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Milliseconds

Range

[1, 100]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.ACCCOMPUTATIONINTERVAL

3150h

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.ACCCOMPUTATIONINTERVAL

3250h

03h

Unsigned8

-

-

Read/Write

No